Part Number: 66AK2H12
Other Parts Discussed in Thread: 66AK2H12
Tool/software: TI-RTOS
Hello,
I have a 66ak2h12, CCS 7.2.0, sdk_rtos_k2hk_4_00_00_04, and pdk_k2hk_4_0_6.
I need to perform an i2c probe to determine what devices are physically connected to each of the 3 busses.
The process is this:
call I2C_init: status OK
Init a params block, bit rate is 400KHz; I have tried blocking and non-blocking
I2C_open (busNo, ¶ms): OK
For each of the 128 possible addresses:
Build a transaction:
write 0 bytes, read 1 byte
slave addr = address
master mode = true
if (blocking mode)
callback function: function which posts to a semaphore
arg = semaphore ID
else
timeout = 2000
status = I2C_transfer (handle, &transaction)
if blocking mode, wait on sem with timeout = 2000
report status
incr device address
close device
I confirmed that there are devices at 0x4f, 0x50, and 0x51 using uBoot. However, the TI-RTOS implementation behaves in this way:
- The first several probes return a status of -3
- The next several probes return a status of 0, after reaching the timeout period
If I start the scan at 0x50, then I get good status for 0x50 and 0x51, followed by the behavior above.
Questions:
- Once the driver detects an ACK error, is there some recovery function I need to call to clear the prior transaction, which failed?
- I see there is an I2C command function, and a command for "probe", but that returned an error code indicating it was not implemented. Is that correct?
- Is there a probe example for the RTOS I2C driver which I can examine?
Many thanks,
Tim
The behavior is this: