Part Number: AM3351
Tool/software: Linux
hi, i am using ti-processor-sdk-03.00.00.04 for getting 24 bit LCD display on my am3351 processor based board,
i did pinmuxing as per below i mentioned. but i am not able to find any light or color changes on my display, please suggest me what we need to take care for getting display on lcd.
///// .dts File ///
/*
* Copyright (C) 2012 Texas Instruments Incorporated - http://www.ti.com/
*
* This program is free software; you can redistribute it and/or modify
* it under the terms of the GNU General Public License version 2 as
* published by the Free Software Foundation.
*/
/dts-v1/;
#include "am33xx.dtsi"
#include "am335x-bone-common.dtsi"
#include <dt-bindings/pwm/pwm.h>
#include <dt-bindings/display/tda998x.h>
/ {
model = "TI AM335x BeagleBone Black";
compatible = "ti,am335x-bone-black", "ti,am335x-bone", "ti,am33xx";
backlight {
status = "okay";
compatible = "pwm-backlight";
pwms = <&ehrpwm0 0 50000 0>;
brightness-levels = <
0 1 2 3 4 5 6 7 8 9
10 11 12 13 14 15 16 17 18 19
20 21 22 23 24 25 26 27 28 29
30 31 32 33 34 35 36 37 38 39
40 41 42 43 44 45 46 47 48 49
50 51 52 53 54 55 56 57 58 59
60 61 62 63 64 65 66 67 68 69
70 71 72 73 74 75 76 77 78 79
80 81 82 83 84 85 86 87 88 89
90 91 92 93 94 95 96 97 98 99
100
>;
default-brightness-level = <50>;
};
panel {
compatible = "ti,tilcdc,panel";
status = "okay";
pinctrl-names = "default";
pinctrl-0 = <&nxp_hdmi_bonelt_pins>;
panel-info {
ac-bias = <255>;
ac-bias-intrpt = <0>;
dma-burst-sz = <16>;
bpp = <32>;
fdd = <0x80>;
sync-edge = <0>;
sync-ctrl = <1>;
raster-order = <0>;
fifo-th = <0>;
};
display-timings {
800x480p62 {
clock-frequency = <30000000>;
hactive = <800>;
vactive = <480>;
hfront-porch = <39>;
hback-porch = <39>;
hsync-len = <47>;
vback-porch = <29>;
vfront-porch = <13>;
vsync-len = <2>;
hsync-active = <1>;
vsync-active = <1>;
};
};
};
};
&ldo3_reg {
regulator-min-microvolt = <1800000>;
regulator-max-microvolt = <1800000>;
regulator-always-on;
};
&mmc1 {
vmmc-supply = <&vmmcsd_fixed>;
};
&mmc2 {
vmmc-supply = <&vmmcsd_fixed>;
pinctrl-names = "default";
pinctrl-0 = <&emmc_pins>;
bus-width = <8>;
status = "okay";
};
&cpu0_opp_table {
/*
* All PG 2.0 silicon may not support 1GHz but some of the early
* BeagleBone Blacks have PG 2.0 silicon which is guaranteed
* to support 1GHz OPP so enable it for PG 2.0 on this board.
*/
oppnitro@1000000000 {
opp-supported-hw = <0x06 0x0100>;
};
};
&am33xx_pinmux {
nxp_hdmi_bonelt_pins: nxp_hdmi_bonelt_pins {
pinctrl-single,pins = <
0xa0 0x08 /* lcd_data0.lcd_data0, OMAP_MUX_MODE0 | AM33XX_PIN_OUTPUT | AM33XX_PULL_DISA */
0xa4 0x08 /* lcd_data1.lcd_data1, OMAP_MUX_MODE0 | AM33XX_PIN_OUTPUT | AM33XX_PULL_DISA */
0xa8 0x08 /* lcd_data2.lcd_data2, OMAP_MUX_MODE0 | AM33XX_PIN_OUTPUT | AM33XX_PULL_DISA */
0xac 0x08 /* lcd_data3.lcd_data3, OMAP_MUX_MODE0 | AM33XX_PIN_OUTPUT | AM33XX_PULL_DISA */
0xb0 0x08 /* lcd_data4.lcd_data4, OMAP_MUX_MODE0 | AM33XX_PIN_OUTPUT | AM33XX_PULL_DISA */
0xb4 0x08 /* lcd_data5.lcd_data5, OMAP_MUX_MODE0 | AM33XX_PIN_OUTPUT | AM33XX_PULL_DISA */
0xb8 0x08 /* lcd_data6.lcd_data6, OMAP_MUX_MODE0 | AM33XX_PIN_OUTPUT | AM33XX_PULL_DISA */
0xbc 0x08 /* lcd_data7.lcd_data7, OMAP_MUX_MODE0 | AM33XX_PIN_OUTPUT | AM33XX_PULL_DISA */
0xc0 0x08 /* lcd_data8.lcd_data8, OMAP_MUX_MODE0 | AM33XX_PIN_OUTPUT | AM33XX_PULL_DISA */
0xc4 0x08 /* lcd_data9.lcd_data9, OMAP_MUX_MODE0 | AM33XX_PIN_OUTPUT | AM33XX_PULL_DISA */
0xc8 0x08 /* lcd_data10.lcd_data10, OMAP_MUX_MODE0 | AM33XX_PIN_OUTPUT | AM33XX_PULL_DISA */
0xcc 0x08 /* lcd_data11.lcd_data11, OMAP_MUX_MODE0 | AM33XX_PIN_OUTPUT | AM33XX_PULL_DISA */
0xd0 0x08 /* lcd_data12.lcd_data12, OMAP_MUX_MODE0 | AM33XX_PIN_OUTPUT | AM33XX_PULL_DISA */
0xd4 0x08 /* lcd_data13.lcd_data13, OMAP_MUX_MODE0 | AM33XX_PIN_OUTPUT | AM33XX_PULL_DISA */
0xd8 0x08 /* lcd_data14.lcd_data14, OMAP_MUX_MODE0 | AM33XX_PIN_OUTPUT | AM33XX_PULL_DISA */
0xdc 0x08 /* lcd_data15.lcd_data15, OMAP_MUX_MODE0 | AM33XX_PIN_OUTPUT | AM33XX_PULL_DISA */
0xe0 0x00 /* lcd_vsync.lcd_vsync, OMAP_MUX_MODE0 | AM33XX_PIN_OUTPUT */
0xe4 0x00 /* lcd_hsync.lcd_hsync, OMAP_MUX_MODE0 | AM33XX_PIN_OUTPUT */
0xe8 0x00 /* lcd_pclk.lcd_pclk, OMAP_MUX_MODE0 | AM33XX_PIN_OUTPUT */
0xec 0x00 /* lcd_ac_bias_en.lcd_ac_bias_en, OMAP_MUX_MODE0 | AM33XX_PIN_OUTPUT */
0x3c 0x09 /* lcd_data16.lcd_data16, OMAP_MUX_MODE1 | AM33XX_PIN_OUTPUT | AM33XX_PULL_DISA */
0x38 0x09 /* lcd_data17.lcd_data17, OMAP_MUX_MODE1 | AM33XX_PIN_OUTPUT | AM33XX_PULL_DISA */
0x34 0x09 /* lcd_data18.lcd_data18, OMAP_MUX_MODE1 | AM33XX_PIN_OUTPUT | AM33XX_PULL_DISA */
0x30 0x09 /* lcd_data19.lcd_data19, OMAP_MUX_MODE1 | AM33XX_PIN_OUTPUT | AM33XX_PULL_DISA */
0x2c 0x09 /* lcd_data20.lcd_data20, OMAP_MUX_MODE1 | AM33XX_PIN_OUTPUT | AM33XX_PULL_DISA */
0x28 0x09 /* lcd_data21.lcd_data21, OMAP_MUX_MODE1 | AM33XX_PIN_OUTPUT | AM33XX_PULL_DISA */
0x24 0x09 /* lcd_data22.lcd_data22, OMAP_MUX_MODE1 | AM33XX_PIN_OUTPUT | AM33XX_PULL_DISA */
0x20 0x09 /* lcd_data23.lcd_data23, OMAP_MUX_MODE1 | AM33XX_PIN_OUTPUT | AM33XX_PULL_DISA */
>;
};
nxp_hdmi_bonelt_off_pins: nxp_hdmi_bonelt_off_pins {
pinctrl-single,pins = <
0x1b0 0x03 /* xdma_event_intr0, OMAP_MUX_MODE3 | AM33XX_PIN_OUTPUT */
>;
};
ehrpwm0_pins: backlight_pins {
pinctrl-single,pins = <
0x164 ( PIN_OUTPUT_PULLUP | MUX_MODE3 ) /* (U14) gpmc_a2.ehrpwm1A */
>;
};
mcasp0_pins: mcasp0_pins {
pinctrl-single,pins = <
AM33XX_IOPAD(0x9ac, PIN_INPUT_PULLUP | MUX_MODE0) /* mcasp0_ahcklx.mcasp0_ahclkx */
AM33XX_IOPAD(0x99c, PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* mcasp0_ahclkr.mcasp0_axr2*/
AM33XX_IOPAD(0x994, PIN_OUTPUT_PULLUP | MUX_MODE0) /* mcasp0_fsx.mcasp0_fsx */
AM33XX_IOPAD(0x990, PIN_OUTPUT_PULLDOWN | MUX_MODE0) /* mcasp0_aclkx.mcasp0_aclkx */
AM33XX_IOPAD(0x86c, PIN_OUTPUT_PULLDOWN | MUX_MODE7) /* gpmc_a11.GPIO1_27 */
>;
};
};
&lcdc {
status = "okay";
port {
lcdc_0: endpoint@0 {
remote-endpoint = <&hdmi_0>;
};
};
};
&i2c0 {
hdmi1: hdmi@70 {
compatible = "nxp,tda998x";
reg = <0x70>;
};
};
&i2c0 {
tda19988: tda19988 {
compatible = "nxp,tda998x";
reg = <0x70>;
pinctrl-names = "default", "off";
pinctrl-0 = <&nxp_hdmi_bonelt_pins>;
pinctrl-1 = <&nxp_hdmi_bonelt_off_pins>;
#sound-dai-cells = <0>;
audio-ports = < AFMT_I2S 0x03>;
ports {
port@0 {
hdmi_0: endpoint@0 {
remote-endpoint = <&lcdc_0>;
};
};
};
};
};
&rtc {
system-power-controller;
};
&epwmss0 {
status = "okay";
ehrpwm0: pwm@48300200{
status = "okay";
pinctrl-names = "default";
pinctrl-0 = <&ehrpwm0_pins>;
};
};
&mcasp0 {
#sound-dai-cells = <0>;
pinctrl-names = "default";
pinctrl-0 = <&mcasp0_pins>;
status = "okay";
op-mode = <0>; /* MCASP_IIS_MODE */
tdm-slots = <2>;
serial-dir = < /* 0: INACTIVE, 1: TX, 2: RX */
0 0 1 0
>;
tx-num-evt = <32>;
rx-num-evt = <32>;
};
&sgx {
status = "okay";
};
/ {
clk_mcasp0_fixed: clk_mcasp0_fixed {
#clock-cells = <0>;
compatible = "fixed-clock";
clock-frequency = <24576000>;
};
clk_mcasp0: clk_mcasp0 {
#clock-cells = <0>;
compatible = "gpio-gate-clock";
clocks = <&clk_mcasp0_fixed>;
enable-gpios = <&gpio1 27 0>; /* BeagleBone Black Clk enable on GPIO1_27 */
};
sound {
compatible = "simple-audio-card";
simple-audio-card,name = "TI BeagleBone Black";
simple-audio-card,format = "i2s";
simple-audio-card,bitclock-master = <&dailink0_master>;
simple-audio-card,frame-master = <&dailink0_master>;
dailink0_master: simple-audio-card,cpu {
sound-dai = <&mcasp0>;
clocks = <&clk_mcasp0>;
};
/*simple-audio-card,codec {
sound-dai = <&tda19988>;
};*/
};
};
Thank you.