Tool/software: Linux
Hello,
I am using mcspi ,
I have started testing it, but for some unknown reason, I get that mcspi tx remains full.
In MCSPI_CHxSTAT register txs bit remains 1 , after sending one byte in mcspi.
I use mcspi2, and check register 0x4809a030 (MCSPI_CHxSTAT) :
0x4809a000:
0x4809a000: 0021 0000 0000 0000
0x4809a010: 0015 0001 0005 0000
0x4809a020: 0000 0000 0001 1c3d9
0x4809a030: 0007 0000 0000 0000
Is there any reason why the byte is not being send ?
MCSPI #2 is configured as master.
Regards,
Ran