Part Number: TMDXEVM8148
Tool/software: Linux
Hello,
My requirement is to do a VGA Input Capture on TMDXEVM8148 DM8148 EVM Board and store it to a H264 encoded file, as a quick POC for our client. Is this possible with this EVM Board without making any HW changes? Based upon the datasheet from Mistral we have procured this board.
I have gone through the e2e forums and below 2 threads were revelant to my search
But at the end, im a bit confused.
Kindly clarify my below queries
1. These two forums says VGA capture cannot be done through TVP7002 on this EVM , But as per Mistral's Datasheet on this EVM, it states "This platform supports multiple display outputs such as LCD, HDMI, S-Video and Composite- Video, and inputs such as S-Video and Composite video Component Video, VGA, HDMI, Serial camera, and parallel camera."(it supports VGA input) Kindly clarify which one is valid.
2. If this board supports VGA Capture, Can TI provide any guidelines document or sample program or examples to enable VGA and capture it?
3. From http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/716/p/242232/1135217 , i see "We have TVP5147 for VGA input." But in the schematics of this EVM, TVP5147 has only S-Video and Composite video inputs. It doesnt have VGA as input, and VGA is present with TVP7002 . Can someone please explain how TVP5147 is used in this EVM to capture VGA?
4. If this board doesn't support VGA Capture, Can TI Recommend any other board which has different input capture like VGA,HDMI,DVI,S-Video,Component and Composite?
5.From the Capture and encode example present in the SDK i understand that it captures Component input through TVP7002 . Can TI provide any guidelines on how to change this example to Capture VGA in the omx example?