This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

issue on running demos through command line



hi,

I am trying to display the default demos given by TI(opt/dvsdk/dm6467/data/videos/) through command line for this

 

i had made my setup with RGB wires connected to the component output and HDTV and i booted the kernel through NFS mounted root file system.So, From console i had killed the interface by using (killall -9 interface ) and loaded ./loadmodule.sh successfully and now when i execute the commands like

./decode -v data/videos/dust_1080i_30fps.264

(or)

./decode -v data/videos/ -y 2

(or)

./decode -v data/videos/dust_1080i_30fps.264 -o

 

for every command i can see the output on the console

Decode demo started.
Decode demo ARM Load: 112% DSP Load: 33% Display Type: D1 NTSC Video Codec: H.264 Video fps: 7 fps Video bit rate: 12960 kbps Video resolution: 1920x1080 So

Decode demo ARM Load: 141% DSP Load: 42% Display Type: D1 NTSC Video Codec: H.264 Video fps: 26 fps Video bit rate: 22086 kbps Video resolution: 1920x1080 S

Decode demo ARM Load: 84% DSP Load: 43% Display Type: D1 NTSC Video Codec: H.264 Video fps: 27 fps Video bit rate: 21337 kbps Video resolution: 1920x1080 So

Decode demo ARM Load: 125% DSP Load: 45% Display Type: D1 NTSC Video Codec: H.264 Video fps: 26 fps Video bit rate: 22428 kbps Video resolution: 1920x1080 S

Decode demo ARM Load: 118% DSP Load: 43% Display Type: D1 NTSC Video Codec: H.264 Video fps: 26 fps Video bit rate: 22331 kbps Video resolution: 1920x1080 S

Decode demo ARM Load: 118% DSP Load: 46% Display Type: D1 NTSC Video Codec: H.264 Video fps: 27 fps Video bit rate: 22567 kbps Video resolution: 1920x1080 S

Decode demo ARM Load: 98% DSP Load: 45% Display Type: D1 NTSC Video Codec: H.264 Video fps: 26 fps Video bit rate: 20148 kbps Video resolution: 1920x1080 So

Decode demo ARM Load: 140% DSP Load: 46% Display Type: D1 NTSC Video Codec: H.264 Video fps: 26 fps Video bit rate: 22971 kbps Video resolution: 1920x1080 S

...........................................................

.........................................................

..........................................................

Clip ended, exiting demo..

but i never seen a display on my hdtv..

So,please help on this regards to solve my problem such that i should get display on my hdtv through command line... it will be great help for me

 

Thanks & Regards

Vijay