This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/TMDSEVM572X: Top measuring questions

Part Number: TMDSEVM572X
Other Parts Discussed in Thread: AM5728

Tool/software: Linux

Hi,

In desktop linux I would normally run "top" to see my cpu loading. Using the embedded Linux on the AM5728 EVM I can run top and get a cpu measure. As the AM5728 is dual core for the CPUs I'm not sure if both CPUs were running at max this would return 100% or 200% (irix mode shift+i doesn't seem to do anything which is how I would normally distinguish on a desktop).

I would also likely to know what is the equivalent of "top" to measure DSP core loading? If there isn't a simple command how do people go about measuring DSP loading?

Thanks,

John