Other Parts Discussed in Thread: TFP410, TMS320DM368
Hi,
I am interfacing TFP410 with TMS320DM368 digital video output port. I have the following queries:
TMS320DM368
1. TMS320DM368 data sheet recommends on
(page-21):
“To reduce EMI and reflections, depending on the trace
length, approximately 22 Ω to 50 Ω damping resistors are recommend on
the following outputs
placed near the device: YOUT(0-7),COUT(0-7), HSYNC, VSYNC, LCD_OE, FIELD, and
VCLK.”
Is the
above damping resistors included PCB trace impedance? i.e. if PCB trace
impedance is 10 Ω then damping resistors may
be 12 Ω to 40
Ω ?
2. What about the other Digital Video RGB
signals (GIO33, GIO32, GIO30, GIO29, GIO80,
GIO28 and GIO27), do these signals are also require
damping resistors?