Part Number: TMDSLCDK138
Other Parts Discussed in Thread: OMAP-L138
Tool/software: Linux
Hi!
I started to work with OMAP-L138 LCDK recently.
And i found only an version of MCSK on the SD card from the box, just like you.
I've wasted about a week exploring MCSDK before i realised that newest SDK 04_00.... exists
So i'm trying to boot the board whith Linux from SD card now.
Yes, i've found and read discussion of the same problem on the forum here
But i didn't success.
First, I create an SD card using Win32DiskImager and omapl138-lcdk-linux-04.00.00.04.img
Second, I change SW1 to (1 - off, 2 -off, 3-off, 4 -on).
Then i insert SD card to slot and power up the board.
But nothing happens. There is not any output in console or vga.
So can you check what i'm doing wrong?