Tool/software: Linux
Is the source code available for the Am437x board diagnostics. If so where may I download it from?
Thank Yo
Ed D'Entremont
L3 Technologies
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Linux
Is the source code available for the Am437x board diagnostics. If so where may I download it from?
Thank Yo
Ed D'Entremont
L3 Technologies
We are looking for the board diagnostics that TI runs prior to shipping their boards to reduce the amount of returns. When I look at this site for the AM43xx board http://processors.wiki.ti.com/index.php/AM43xx_Hardware_Diagnostics I see the binary's, but no link to the source. When I look at this site http://processors.wiki.ti.com/index.php/AM335x_Starter_Kit_Diagnostics for the AM335x board, I see a link to the diagnostic software for these boards. I understand that the software for these boards are open source. Thank you Ed
The EVM diagnostics have now been integrated in our Processor SDK RTOS software offering . All board related software can be found in a component called platform development kit (PDK). If you download the latest version of the SDK the diagnostics are located under the folder path pdk_am335x_1_0_8\packages\ti\board\diag
Most diagnostics tests are designed to be loaded and run from SD boot. The documentation on how to build and run the diagnostics is provided here:

For AM437x specifically, you can invoke the build using :
cd pdk_am437x_1_0_8\packages\ti\board\diag make evmAM437x
// For SD boot use "make evmAM437x_sd"
OR
cd pdk_am437x_1_0_8\packages\ti\board\diag
make skAM437x
// For SD boot use "make skAM437x_sd"
Note: Please ensure that you setup SDK build environment as described here:

Regards,
Rahul