Tool/software: Linux
Hi Experts,
I am able to successfully build the am335x-evm arago-core-tisdk-image using Yocto for SDK 04.00.00.04.
What I want to do now is add support for GTK+3 into my build. I've spent a lot of time reading up on yocto/bitbake and looking through the SDK layers and recipes. I need help getting started adding GTK+3. Using bitbake-layers show-recipes I see there are existing recipes for GTK+3 but many of them say (skipped).
My first question is, what does it mean when show-recipes says skipped? I've been googling and not finding a good explanation. Obviously the recipe is being skipped but my question is why? Is it because the packag(s) that's tagged as skipped is not a dependency of any other recipes used in the SDK?
If I want to add support for GTK+3, do I need to create another layer and add recipes there? Or do I modify an existing recipe? I saw there are some packagegroup recipes, would I edit one of those and add a dependency to GTK+3 there? Or, do I edit the gtk+3 recipe? Or, should I be adding a .bbappend somewhere?
I think that once I get started off in the right direction I can make progress.
Thanks