Part Number: CCSTUDIO
Tool/software: Code Composer Studio
Hi,
I need to use USB Full speed on a C5517 device. I'm using CSL library and I'm trying to let CSL_usbCdcTest work on a DSP-BIOS project.
On this step the project simply set the PLL for a 100MHz system clock and open a CDC USB connection.
I have a main function that I use for the initialization, then the program falls on an idle loop.
I have noticed that if I run CSL_usbCdcTest as a function inside the main (before the idle loop starts) I correctly see the enumeration on the PC. If I move the CSL_usbCdcTest outside the main and I let it run as a GEL function the enumeration fails.
Why is this happening?
Do you have examples or suggestions about how to use CSL_usbCdcTest on a DSP Bios project?
Thank you
Stefano