Part Number: AM5728
Tool/software: TI C/C++ Compiler
Hello.
Reading TRM for Sitara AM572x family, I found in paragraph 7.1.2 about dual Cortex-M4 IPU subsystem that each IPU integrates ARMv6 SIMD and digital signal processor (DSP) extensions but when I try to enable SIMD option in Properties->Build->ARM Compiler->Advanced Options->Runtime Model Options I get first an error message as shown in the following picture:
and later, if I launch a compilation, I will get :
error #24018-D: Option --neon is not valid without -mv7A8
gmake: *** [main.obj] Error 1
gmake: Target 'all' not remade because of errors.
So the question is : is it a compiler problem/bug or datasheet is reporting something wrong ?
Let me add that the problem is present in TI's compiler v17.9.0 STS and v16.9.4 LTS.
Thank you and best regards,
Scianni Vincenzo