Hello,
I'm posting this for one of my customers so they can reply directly.
Essentially they are having issues with the performance of our AAC Encoder on the 5509A when using off chip memory. They are experiencing delays and strange sounds when using off chip memory in some instances. Are there any guidelines for this algo in terms of what data/program can go on/off chip or does everything have to be in on chip RAM? Obviously having everything on chip is ideal, but is not the most practical as they are tight for space with their application already. Please let me know much flexibility there is in managing the AAC Encoder algorithm in terms of memory resources to maintain the best performance while using the least internal memory.
Thanks,
Tom