This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6747 is failedwhen it boots from SPI0 Flash

In my C6747 board , I want boot it with SPI0 flash. I failed.

I describe the question with attachment.

Could you help me?

Thank you so much!c6747boot_question.pdf

   

  • Hi,

    I've notified the sw team. Their feedback will be posted here.

    Best Regards,
    Yordan
  • Thanks for describing the details of your problem. Why do you think the boot failed ? You indicate in the document that the LED stays on even when you load the code over the emulator as well as when the application boot from flash.   

    If you suspect that this is a boo tissue then can you perform the following debug steps that will help isolate this issue.

    * Run the debug GEL file provided here when the boot fails and attach the log

    * Reduce to the SPI speed to 10 Mhz and retry the experiment.

    Have you checked the GPIO register to determine that it is set and then unset to blink the LED. Is the timer count setup correctly? If not the LED could be blinking to quickly.

    Regards,

    Rahul

  • Thank you so much for your help.

    And I did as your suggestion. I attach the result.

    And I still has some question,  shown with the attachment.

    Thank you!c6747boot_question_v02.pdf

  • C674X_0: GEL Output: 
    ---------------------------------------------
    C674X_0: GEL Output: |             Device Information            |
    C674X_0: GEL Output: ---------------------------------------------
    C674X_0: GEL Output: DEV_INFO_00 = 0x9B7DF02F
    C674X_0: GEL Output: DEV_INFO_01 = 0x00000000
    C674X_0: GEL Output: DEV_INFO_02 = 0x0000F375
    C674X_0: GEL Output: DEV_INFO_03 = 0x00000004
    C674X_0: GEL Output: DEV_INFO_04 = 0x00000000
    C674X_0: GEL Output: DEV_INFO_05 = 0x000003E0
    C674X_0: GEL Output: DEV_INFO_06 = 0x00000200
    C674X_0: GEL Output: DEV_INFO_07-DEV_INFO_08-DEV_INFO_09-DEV_INFO_10-DEV_INFO_11-DEV_INFO_12 = 8-0-172209-3-43-40
    C674X_0: GEL Output: DEV_INFO_13,DEV_INFO_14,DEV_INFO_15,DEV_INFO_16 = 2,0,0,10475
    C674X_0: GEL Output: -----
    C674X_0: GEL Output: DEV_INFO_17 = 0x00030003
    C674X_0: GEL Output: DEV_INFO_18 = 0x00000000
    C674X_0: GEL Output: DEV_INFO_19 =C674X_0: GEL Output: 0C674X_0: GEL Output: 0C674X_0: GEL Output: 0C674X_0: GEL Output: 0C674X_0: GEL Output: 0C674X_0: GEL Output: 
    C674X_0: GEL Output: -----
    C674X_0: GEL Output: DEV_INFO_20 = 0x30303864
    C674X_0: GEL Output: DEV_INFO_21 = 0x3530306B
    C674X_0: GEL Output: DEV_INFO_22 = 0x00000000
    C674X_0: GEL Output: DEV_INFO_23 = 0x00000000
    C674X_0: GEL Output: -----
    C674X_0: GEL Output: DEV_INFO_24 = 0x0302802B
    C674X_0: GEL Output: DEV_INFO_25 = 0x0802A0B1
    C674X_0: GEL Output: DEV_INFO_06 = 0x00000200
    C674X_0: GEL Output: DEV_INFO_26 = 0x51D60002
    C674X_0: GEL Output: 
    
    C674X_0: GEL Output: ---------------------------------------------
    C674X_0: GEL Output: |               BOOTROM Info                |
    C674X_0: GEL Output: ---------------------------------------------
    C674X_0: GEL Output: ROM ID: d800k005 
    C674X_0: GEL Output: Silicon Revision 3.0
    C674X_0: GEL Output: Boot pins: 62325
    C674X_0: GEL Output: Boot Mode: SPI0 Flash (0x0000F375)
    C674X_0: GEL Output: 
    ROM Status Code: 0x00000000 
    Description:C674X_0: GEL Output: No error
    C674X_0: GEL Output: 
    Program Counter (PC) = 0x00712144
    C674X_0: GEL Output: 
    C674X_0: GEL Output: ---------------------------------------------
    C674X_0: GEL Output: |              Clock Information             |
    C674X_0: GEL Output: ---------------------------------------------
    C674X_0: GEL Output: 
    C674X_0: GEL Output: PLLs configured to utilize crystal.
    C674X_0: GEL Output: ASYNC3 = PLL0_SYSCLK2
    C674X_0: GEL Output: 
    C674X_0: GEL Output: NOTE:  All clock frequencies in following PLL sections are based
    C674X_0: GEL Output: off OSCIN = 24 MHz.  If that value does not match your hardware
    C674X_0: GEL Output: you should change the #define in the top of the gel file, save it,
    C674X_0: GEL Output: and then reload.
    C674X_0: GEL Output: 
    C674X_0: GEL Output: ---------------------------------------------
    C674X_0: GEL Output: |              PLL0 Information             |
    C674X_0: GEL Output: ---------------------------------------------
    C674X_0: GEL Output: 
    C674X_0: GEL Output: PLL0_SYSCLK1 = 300 MHz
    C674X_0: GEL Output: PLL0_SYSCLK2 = 150 MHz
    C674X_0: GEL Output: PLL0_SYSCLK3 = 100 MHz
    C674X_0: GEL Output: PLL0_SYSCLK4 = 75 MHz
    C674X_0: GEL Output: PLL0_SYSCLK5 = 50 MHz
    C674X_0: GEL Output: PLL0_SYSCLK6 = 300 MHz
    C674X_0: GEL Output: PLL0_SYSCLK7 = 37 MHz
    C674X_0: GEL Output: 
    C674X_0: GEL Output: ---------------------------------------------
    C674X_0: GEL Output: |              PSC0 Information             |
    C674X_0: GEL Output: ---------------------------------------------
    C674X_0: GEL Output: 
    C674X_0: GEL Output: State Decoder:
    C674X_0: GEL Output:  0 = SwRstDisable (reset asserted, clock off)
    C674X_0: GEL Output:  1 = SyncReset (reset assered, clock on)
    C674X_0: GEL Output:  2 = Disable (reset de-asserted, clock off)
    C674X_0: GEL Output:  3 = Enable (reset de-asserted, clock on)
    C674X_0: GEL Output: >3 = Transition in progress
    C674X_0: GEL Output: 
    C674X_0: GEL Output: Module 0:	EDMA3CC (0)        STATE = 3
    C674X_0: GEL Output: Module 1:	EDMA3 TC0          STATE = 3
    C674X_0: GEL Output: Module 2:	EDMA3 TC1          STATE = 3
    C674X_0: GEL Output: Module 3:	EMIFA (BR7)        STATE = 3
    C674X_0: GEL Output: Module 4:	SPI 0              STATE = 3
    C674X_0: GEL Output: Module 5:	MMC/SD 0           STATE = 3
    C674X_0: GEL Output: Module 6:	AINTC              STATE = 3
    C674X_0: GEL Output: Module 7:	ARM RAM/ROM        STATE = 3
    C674X_0: GEL Output: Module 9:	UART 0             STATE = 3
    C674X_0: GEL Output: Module 10:	SCR 0 (BR0/1/2/8)  STATE = 3
    C674X_0: GEL Output: Module 11:	SCR 1 (BR4)        STATE = 3
    C674X_0: GEL Output: Module 12:	SCR 2 (BR3/5/6)    STATE = 3
    C674X_0: GEL Output: Module 13:	PRUSS              STATE = 3
    C674X_0: GEL Output: Module 14:	ARM                STATE = 0
    C674X_0: GEL Output: Module 15:	DSP                STATE = 3
    C674X_0: GEL Output: 
    C674X_0: GEL Output: ---------------------------------------------
    C674X_0: GEL Output: |              PSC1 Information             |
    C674X_0: GEL Output: ---------------------------------------------
    C674X_0: GEL Output: 
    C674X_0: GEL Output: State Decoder:
    C674X_0: GEL Output:  0 = SwRstDisable (reset asserted, clock off)
    C674X_0: GEL Output:  1 = SyncReset (reset assered, clock on)
    C674X_0: GEL Output:  2 = Disable (reset de-asserted, clock off)
    C674X_0: GEL Output:  3 = Enable (reset de-asserted, clock on)
    C674X_0: GEL Output: >3 = Transition in progress
    C674X_0: GEL Output: 
    C674X_0: GEL Output: Module 1:	USB0 (2.0)         STATE = 3
    C674X_0: GEL Output: Module 2:	USB1 (1.1)         STATE = 3
    C674X_0: GEL Output: Module 3:	GPIO               STATE = 3
    C674X_0: GEL Output: Module 4:	UHPI               STATE = 3
    C674X_0: GEL Output: Module 5:	EMAC               STATE = 3
    C674X_0: GEL Output: Module 6:	EMIFB (BR20)       STATE = 3
    C674X_0: GEL Output: Module 7:	MCASP0 + FIFO      STATE = 3
    C674X_0: GEL Output: Module 8:	MCASP1 + FIFO      STATE = 3
    C674X_0: GEL Output: Module 9:	MCASP2 + FIFO      STATE = 3
    C674X_0: GEL Output: Module 10:	SPI 1              STATE = 3
    C674X_0: GEL Output: Module 11:	I2C 1              STATE = 3
    C674X_0: GEL Output: Module 12:	UART 1             STATE = 3
    C674X_0: GEL Output: Module 13:	UART 2             STATE = 3
    C674X_0: GEL Output: Module 16:	LCDC               STATE = 3
    C674X_0: GEL Output: Module 17:	eHRPWM (all)       STATE = 3
    C674X_0: GEL Output: Module 20:	eCAP (all)         STATE = 3
    C674X_0: GEL Output: Module 21:	eQEP 0/1           STATE = 3
    C674X_0: GEL Output: Module 24:	SCR8 (Br15)        STATE = 3
    C674X_0: GEL Output: Module 25:	SCR7 (Br12)        STATE = 3
    C674X_0: GEL Output: Module 26:	SCR12 (Br18)       STATE = 3
    C674X_0: GEL Output: Module 31:	L3 RAM (Br13)      STATE = 3
    I do as "Run the debug GEL file", the  log file is shown as the attachment"gel_log.txt".  Does it means anything?

  • Thank you very much!

    I have another question, could you help me again?

  • From the log it appears, the device is still held inside ROM bootloader and has not exited. The device clocks are setup correctly to 300 MHz but the device seems to be held in the start condition without any error. Have you put a scope on the SPI clk to see if the clock and data transfer starts from flash ? did you try the experiment of slowing down the SPI clock to 10MHz.

    Can you try the SPI boot image on TI evaluation platform before testing it on your custom board.

    You can post all your questions here and we would be glad to help.

    Regards,
    Rahul
  • Rahul Prabhu said:
    did you try the experiment of slowing down the SPI clock to 10MHz.

    Yes, I  changed the SPI0 CLK to be 10MHz in AISgen. But I set the SPI1 CLK  1MHz in my LED application. May the SPI1 clk affect the SPI0 flash boot?

    What a pitty, the TI evaluation platform of C6747 is not on my hand. 

    Rahul Prabhu said:
    Have you put a scope on the SPI clk to see if the clock and data transfer starts from flash ?

    I put the scope  on tge SPI0 clk, and there is no SPI0 CLK is output. What may be the reason?

    I did not find the codes for SPI0 register settings in spiflash_writer_dsp projection.

    Where is the SPI0 clk frequency set, is it set in AISgen? 

    Thank you so much!

  • I read the map file of my LED project.

    I find  the address of  _c_int00 is 0080e080, shown as following:  

     

    And I find the entrypoin in spi_writer_dsp(or AISgen) is 0xc1080000, shown as the following:

    Must both of the address be the same?

  • Rahul, Could you help me again about aboved question?

  • No the entry point of the application and the flash writer doesn`t have to be the same. Can you load your led program into L2 or shared RAM on the chip and see if that makes a difference. We provide a SPI boot example and the steps and code for reference herE:
    processors.wiki.ti.com/.../Boot_Images_for_OMAP-L137

    You can look at the instructions specific to the C6747 EVM for reference to see if you can identify any issues.

    Regards,
    Rahul