Hi,
Based on:
http://wiki.davincidsp.com/images/a/a5/ArmETBv2.pdf
and
http://www.tiexpressdsp.com/index.php/ETB
I purchased an Blackhawk USB560m emulator, and am now trying to set it up.
After I select the Blackhawk USB560m - DM6446 Emulator in CCS sestup, I have only the ARM and DSP processors. So I have been trying to figure out how to get the ETB as well. If I try to add the ETB11 from the create board page, I get the following error: The board can only support one processor with this type.
If I remove the arm and add the ETB11, I get an error of: TMS470RX is not supported. Please re-install Code composer or select a different driver.
At this point I am confused. :)
Can someone tell me what I am missing or doing wrong?
Thanks!
Mike