Part Number: TMS320VC5507
Tool/software: Code Composer Studio
HI everybody,
I'm working on a digital signal processing project based on TMS320VC5507. I didn't add CSL files to my project and I want to know that if it is possible or not?
Because under the C55XCSL download tap, the devices which are supported by CSL are mentioned and 5507 does not exist in this list.
This is the matter I am searching for it.
Could I use this API for my project based on 5507?
Is there any way to this? .
If not could anyone help me to understand the description of C55XCSL.
C55XCSL Description:
The C55x CSL provides an API for configuring and controlling the on-chip peripherals for easy compatibility between various C55x devices.
Thanks,