Other Parts Discussed in Thread: TVP5158, TVP5146
According to the DM365 data sheet, the CIN[7..0] bus can be used in YCC 08-bit mode which allows for 2 simultaneous decoder inputs with the CIN bus being the "upper" channel and the YIN bus being the lower channel.
This would be perfect for me as I'm planning on hooking up two decoders (synchronized to the same master clock) in BT656 mode and would like to avoid multiplexing them byte wise as done in other reference designs using the TVP5158.
My software group is insisting that this can not be done, as there are no drivers to support this. Does anyone know if this is true? Do I actualy have to multiplex the two inputs so that they can be demultiplexed internally? With all the flexibility designed into the VPFE (ie swapping busses, running 8 or 16 bits with or without embedded sync, etc.) I find it extremely hard to believe.
Thanks for your help!