Part Number: TDA3XEVM
Tool/software: TI-RTOS
Hi,
I have a query regarding loading Appimage from SD card. I have refereed the tda3xx user guide. It is mention in section "3.6 Load using QSPI and SD boot". I have followed the steps given in document but some how Appimage is not loaded into core. I am attaching Putty log bellow please refer and guide.
Note- I am using vision sdk 3.0
=~=~=~=~=~=~=~=~=~=~=~= PuTTY log 2017.11.07 17:29:48 =~=~=~=~=~=~=~=~=~=~=~=
TDA3xx SBL Boot
Identified 15X15 Silicon
DPLL Configuration Completed
Clock Domain Configuration Completed
Module Enable Configuration Completed
TI EVM PAD Configuration Completed
DDR Configuration Completed
TDA3xx SOC Init Completed
App Image Download Begins
Manufacturer ID - 0x20
Device ID - 0xBA
Invalid Magic String in MultiCore Image
Valid App Image is not Available
EVE MMU configuration completed
*****************************************************************
32K Timer is used to measure cycles, divide by 32K to get time in seconds
Reset to SBL Init Cycles - 1739 (53.07 ms)
SBL Initial Config Cycles - 225 (6.86 ms)
SOC Init Cycles - 469 (14.31 ms)
DDR Config Clock Cycles - 229 (6.98 ms)
App Image Load Cycles - 463 (14.12 ms)
Slave Core Bootup Cycles - 114 (3.47 ms)
SBL Boot-up Cycles - 1502 (45.83 ms)
*****************************************************************
No IPU1 CPU1 App Found, Switching to while Loop
Regards,
Swapnil