Other Parts Discussed in Thread: AM5728
Tool/software: Linux
I am using the TI AM57xx Sitara board. But after running the kmemleak, I am getting the following memory leaks in the kernel. The Linux kernel version is 4.9.28 and TI SDK is ti-processor-sdk-linux-am57xx-evm-04.00.00.04 . What is the reason for this leaks and how to remove them?
root@am57xx-evm:~# cat /sys/kernel/debug/kmemleak
unreferenced object 0xedc16e00 (size 64):
comm "swapper/0", pid 1, jiffies 4294937364 (age 455.870s)
hex dump (first 32 bytes):
44 18 05 c1 00 00 00 00 01 00 00 00 01 00 00 00 D...............
00 00 00 00 44 18 05 c1 cc d3 01 c1 cc d3 01 c1 ....D...........
backtrace:
[<c031d590>] __kmalloc+0x194/0x210
[<c0391438>] __register_sysctl_table+0x58/0x630
[<c0391a30>] register_sysctl+0x20/0x24
[<c0e132a4>] user_namespace_sysctl_init+0x1c/0x48
[<c02017bc>] do_one_initcall+0x4c/0x178
[<c0e00f68>] kernel_init_freeable+0x1d8/0x268
[<c08c6550>] kernel_init+0x10/0x110
[<c0207c88>] ret_from_fork+0x14/0x2c
[<ffffffff>] 0xffffffff
unreferenced object 0xd5650000 (size 1024):
comm "kworker/0:0", pid 4, jiffies 4294938272 (age 446.860s)
hex dump (first 32 bytes):
01 00 00 52 01 00 00 52 01 00 00 52 01 00 00 52 ...R...R...R...R
01 00 00 52 01 00 00 52 01 00 00 52 01 00 00 52 ...R...R...R...R
backtrace:
[<c031d9c4>] kmem_cache_alloc+0x174/0x1d8
[<c05b8214>] iopte_alloc+0x5c/0xc8
[<c05b888c>] iopte_alloc_large+0x34/0xb4
[<c05b8160>] omap_iommu_map+0x1a0/0x1f8
[<c05b559c>] iommu_map+0x10c/0x180
[<bf0354b8>] rproc_handle_devmem+0x7c/0x12c [remoteproc]
[<bf035890>] rproc_handle_resources+0x64/0xe8 [remoteproc]
[<bf036cac>] __rproc_boot+0x1c4/0x5bc [remoteproc]
[<bf0370d0>] rproc_auto_boot_callback+0x18/0x24 [remoteproc]
[<c0637a90>] request_firmware_work_func+0x44/0x6c
[<c024483c>] process_one_work+0x1dc/0x3f8
[<c0245494>] worker_thread+0x58/0x574
[<c024a7cc>] kthread+0x100/0x118
[<c0207c88>] ret_from_fork+0x14/0x2c
[<ffffffff>] 0xffffffff
unreferenced object 0xd5650800 (size 1024):
comm "kworker/0:0", pid 4, jiffies 4294938272 (age 446.860s)
hex dump (first 32 bytes):
01 00 00 52 01 00 00 52 01 00 00 52 01 00 00 52 ...R...R...R...R
01 00 00 52 01 00 00 52 01 00 00 52 01 00 00 52 ...R...R...R...R
backtrace:
[<c031d9c4>] kmem_cache_alloc+0x174/0x1d8
[<c05b8214>] iopte_alloc+0x5c/0xc8
[<c05b888c>] iopte_alloc_large+0x34/0xb4
[<c05b8160>] omap_iommu_map+0x1a0/0x1f8
[<c05b559c>] iommu_map+0x10c/0x180
[<bf0354b8>] rproc_handle_devmem+0x7c/0x12c [remoteproc]
[<bf035890>] rproc_handle_resources+0x64/0xe8 [remoteproc]
[<bf036cac>] __rproc_boot+0x1c4/0x5bc [remoteproc]
[<bf0370d0>] rproc_auto_boot_callback+0x18/0x24 [remoteproc]
[<c0637a90>] request_firmware_work_func+0x44/0x6c
[<c024483c>] process_one_work+0x1dc/0x3f8
[<c0245494>] worker_thread+0x58/0x574
[<c024a7cc>] kthread+0x100/0x118
[<c0207c88>] ret_from_fork+0x14/0x2c
[<ffffffff>] 0xffffffff
unreferenced object 0xd5651000 (size 1024):
comm "kworker/0:0", pid 4, jiffies 4294938272 (age 446.860s)
hex dump (first 32 bytes):
01 00 30 40 01 00 30 40 01 00 30 40 01 00 30 40 ..0@..0@..0@..0@
01 00 30 40 01 00 30 40 01 00 30 40 01 00 30 40 ..0@..0@..0@..0@
backtrace:
[<c031d9c4>] kmem_cache_alloc+0x174/0x1d8
[<c05b8214>] iopte_alloc+0x5c/0xc8
[<c05b888c>] iopte_alloc_large+0x34/0xb4