Part Number: AM3358
Other Parts Discussed in Thread: AMIC110
The AM3358 is specified for operation at 19.2, 24, 25 & 26MHz but within the TRM generally uses operation at 24MHz as the basis of discussion
There are a couple of interfaces which are identified as being affected if the clock frequency is not 24MHz, namely the ADC and McASP interfaces.
We donot use either of these interfaces but I have been requested to confirm that there are no other restrictions.
Using AM3358BGCZA80EP @ 25MHz on custom Hardware
Any help gratefully received