Tool/software: Code Composer Studio
I use DSP IC is TMS320C5505,Our EEPROM two Boot startup program is completed; SPI module, IIC module and other peripheral read write programs can be normal boot, including the serial port can also be a normal boot. The question is when using DMA to send serial procedures in debug mode work normal, but ,serial port using DMA module to send failure in boot mode, when connect emulator to my board ,the program has been loop in judge is DMA sends complete ,but when connect emulator ,clicking the “run” button, can be a normal work.
My ccs version is 6.2.0.00050, emulator is SEED-XDS560PLUS.