This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROC_start failed



Hi,

I try to create an image compression application using dsplink based on readwrite dsplink example from TI.

The C++ codec is using exceptions, I linked the rts64plus_eh.lib  but I get this error when running application.

============= Sample Application : READWRITE ==========                        
Entered RDWR_Create ()                                                         
DSP-side configuration mismatch/failure                                        
0                        -> success                                                      
Positive value -> DSP-side failure code.                                       
(Uint32) -1       -> DSP-side component was not initialized.                      
                                                                               
    ProcId received : -1, Expected : 0                                         
    DRV configuration status      [0xffffffff]                                   
    IPS configuration status        [0xffffffff]                                   
    POOL configuration status   [0xffffffff]                                   
    MPCS configuration status   [0xffffffff]                                   
    MPLIST configuration status [0xffffffff]                                   
    MQT configuration status       [0xffffffff]                                   
    RINGIO configuration status [0xffffffff]                                   
PROC_start failed. Status: [0x80008052]                                        
Leaving RDWR_Create ()                                                         
Create phase failed. Status: [0x80008052]                                      
Entered RDWR_Delete ()                                                         
Assertion failed (IS_VALID_MSGQ (msgqQueue)). File : msgq.c Line : 478         
MSGQ_release () failed. Status = [0x8000800b]                                  
MSGQ_transportClose () failed. Status = [0x80008000]                           
Leaving RDWR_Delete ()

 

I'm using Ubuntu 10.4 and TI MAKE system to build sources using DSPLink,  both for GPP and DSP

EVM : DM6467T

CCSv 4.1

DSPLink 1.64

DVSDK 3.1

C6000 7.0.1 compiler

Windows 7 pro 64 bits

Any help would be great

Thanks,

CC