Part Number: DRA726
Tool/software: Linux
I am having some issues with smart update. When I try to do an update it tells me that there is nothing to update.
I can install program if they are not already installed.It cannot reinstal as it says that it is already installed.
Using rpm -q I can see that the program that I want to update is a different version than the one to install.
When I check to see if smart is aware that the program is installed it tells me that it is not installled but when I try to install it it tells me that there would be a conflict and list the program that it just told me was not installed plus conflicts that would occur with virtually every programs that are installed.
root@actia-global-display:~/work/rpm-files-update# smart update
Loading cache...
Updating cache... ###################################################################################################################### [100%]
Updating cache... ###################################################################################################################### [100%]
Channels have no new packages.
root@actia-global-display:~/work/rpm-files-update# smart fix
Loading cache...
Updating cache... ###################################################################################################################### [100%]
Computing transaction...
No problems to resolve!
root@actia-global-display:~/work/rpm-files-update# smart upgrade activision
Loading cache...
Updating cache... ###################################################################################################################### [100%]
warning: 'activision' matches no installed packages
Computing transaction...
No interesting upgrades available.
root@actia-global-display:~/work/rpm-files-update# rpm -q activision
activision-1.0+r1036-r0.armv7ahf_neon
root@actia-global-display:~/work/rpm-files-update# smart upgrade activision-1.0+r1036-r0.armv7ahf_neon
Loading cache...
Updating cache... ###################################################################################################################### [100%]
error: 'activision-1.0+r1036-r0.armv7ahf_neon' matches no packages
root@actia-global-display:~/work/rpm-files-update# smart reinstall activision
Loading cache...
Updating cache... ###################################################################################################################### [100%]
warning: 'activision' matches no installed packages
Computing transaction...
root@actia-global-display:~/work/rpm-files-update# smart install activision
Loading cache...
Updating cache... ###################################################################################################################### [100%]
Computing transaction...
Installing packages (78):
activision libc6 libevdev libjpeg62 libstm32-0 pam-plugin-env pam-plugin-securetty udev
base-files libcairo2 libexpat1 libkmod2 libtinfo5 pam-plugin-faildelay pam-plugin-shells update-alternatives-opkg
base-passwd libcan0 libffi6 libnmea0183-0 libudev1 pam-plugin-group pam-plugin-unix update-rc.d
bash libcap2 libfontconfig1 libpam libuuid1 pam-plugin-lastlog pam-plugin-warn util-linux-sulogin
ca-certificates libcrypto1.0.0 libfreetype6 libpam-runtime libxkbcommon0 pam-plugin-limits shadow wayland
curl libcurl4 libgbm2 libpcan0 libz1 pam-plugin-mail shadow-base weston
fontconfig-utils libdrm-omap1 libgcc-s1 libpixman-1-0 mtdev pam-plugin-motd shadow-securetty weston-conf
libacl1 libdrm2 libgpio0 libpng16-16 ncurses-terminfo-base pam-plugin-nologin ti-ipc xkeyboard-config
libattr1 libee0 libinput libssl1.0.0 openssl-conf pam-plugin-permit ti-sgx-ddk-um
libblkid1 liberation-fonts libipu1-0 libstdc++6 pam-plugin-deny pam-plugin-rootok ti-sgx-ddk-um-plugins
28.8MB of package files are needed. 60.8MB will be used.
Confirm changes? (Y/n): Y
Committing transaction...
Preparing... ###################################################################################################################### [ 0%]
error: package update-alternatives-opkg-0.1.8+git0+53274f0875-r0.armv7ahf_neon is already installed
error: package weston-conf-1.9.0-r2.actia_global_display is already installed
error: package shadow-securetty-4.2.1-r3.arago0.actia_global_display is already installed
all 78 packages listed with similar error message
Michel Catudal
ACTIA Corp