Part Number: TMS320C6747
Hello,
I am writing programs in CSL, because I see no CSL example about PSC and pin multiplexing settings, I have no relevant settings in their own procedures, in the view of the value of the register, Found that the corresponding bit really set up. (I use C6747, UART interrupt receive data. Pdk_omapl137_1_0_1 \ package \ TI \ CSL)
What I want to know is:
1. PSC and pin multiplexing are not set in the CSL? If you need to set, I did not find the function of the pin multiplexing settings
2.If I want to set up the PLLC, can I use functions?I also did not find the relevant function in the CSL.
3.Why some folders only header files without source files. like \pdk_omapl137_1_0_1\packages\ti\csl\src\ip\pllc