I am wanting to attach a DAC to the C5505 chip and I just want to make sure I am getting things straight. If I was wanting to use SPI port for a 5MHz DAC with 12 bits, I would not be able to do so. This is because the SPI's clock runs its fastest at 25MHz which could handle 5 bits. Is this all correct?