Tool/software: Linux
I have copied ti-processor-sdk-linux-am437x-evm-01.00.03-Linux-x86-install.bin from the "Start Here" directory on the Micro SD card that comes with the EVM module. On 2 Ubuntu 14.? laptops and 1 Debian 9 laptops when I execute this file it just come back with the prompt, not error message. I also tried it with sudo, same results. If I execute it on a Debian 8.9 version, it installs the SDK properly. All machines and OS's are 64 bit. Has anyone seen this before and what is the fix? Thanks Ed