Part Number: OMAP-L138
hi yordan
OMAP-L138 EVM KIT is under review and testing
I will review the OMAP-L138 Technical Reference Manual and ask a question
I want to use ITU-BT.1120 and SMTPE 296 formats.
ITU-BT.1120 16-bit circuit is not configured in EVM KIT
So I am using ITU-BT.656 circuit configuration in EVM KIT.
However, the L-138 Technical Reference Manual ITU-BT.656 format is SD Video with embedded timing codes
My camera output is HDTV with embedded timing codes in ITU-BT.656 format and the clock is 148.5Mhz.
I would like to know if the ITU-BT.656 format can use HDTV Video with embedded timing codes.
If there is a way, please reply.
and OMAP-L138 Manual TV System Format TABLE describes that Square pixel common image format supports 1080-30p
I want to know if it supports FULL HD[1920X1080P]
Thank you