This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5708: IBIS model for GPMC_WEn

Part Number: AM5708
Other Parts Discussed in Thread: AM5728

Hi,

I need to use IBIS model to simulate the WE signal ( PCB trace ) of the asynchronies emif , AM5728 CPU pin M3 (gpmc_wen) is a driver.

Voltage of the asynchronies interface is set to 3.3V

Which model I need to use,  Model_172, Model_173, Model_174 or Model_175?

Model_172 I/O,3.3V,40D CLASS MODE FAST MODE,IND,10 PERCENT%,BC40D_H_10P_!SC1_3P3
Model_173 I/O,3.3V,40C CLASS MODE SLOW MODE,IND,10 PERCENT%,BC40D_H_10P_SC1_3P3
Model_174 I/O,3.3V,40D CLASS MODE FAST MODE,IND,5 PERCENT%,BC40D_H_5P_!SC1_3P3
Model_175 I/O,3.3V,40C CLASS MODE SLOW MODE,IND,5 PERCENT%,BC40D_H_5P_SC1_3P3

What is the difference between the models?

Thank you ,

Andrzej D