Hi,
I have written a costum driver using gadgetfs with this I can only reach a Throughput of about 25Mbyte/sec and the Systemload is 30% the rest is Idle. I wonder if I would get better performance writing a kernel mode driver since the load in only 30%. What is the maximum Throughput I can get with the current Linux USB Drivers?