This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA2HG: PPLs and lock bits

Part Number: TDA2HG

Dear

 

I would like to know which PLLs have a bit indicating when there are locked. 

We have several PLLs for TD2E and TDA2H.

We see nine  Power supply for PPL (see below)

For each device, please could tell us which one have these bits.

Thank you.

Inline images 1

Inline images 2

  • Hi, ,

    Please, re-attach the images. Now they can't be seen.

    Regards,
    Mariya
  • Just to add, the bit that controls the state, including LOCK state, is DPLL_EN bit, Each DPLL has its own register. For the registers name check Internal Clock Sources and Generators sub-chapter in TRM book.
    Regards,
    Mariya
  • Dear,

    Thank you for the prompt answer.
    Here below what we have for the TDA2E and TDA2H.

    If i understood well, we should have a" Lock" bit for all DPPL listed (when cores are used).

    For APLL_PCIE, [lease how we know if the PLL is lock or not before starting the software?
    Thank you.



    For TDA 2E:

    • DPLL_MPU: It supplies the MPU subsystem clocking internally.
    • DPLL_IVA: It feeds the IVA subsystem clocking.
    • DPLL_CORE: It supplies all interface clocks and also few module functional clocks.
    • DPLL_PER: It supplies several clock sources: a 192-MHz clock for the display functional clock, a
    96-MHz functional clock to subsystems and peripherals.
    • DPLL_ABE: It provides clocks to various modules within the device.
    • DPLL_USB: It provides 960M clock for USB modules (USB1/2/3/4).
    • DPLL_GMAC: It supplies several clocks for the Gigabit Ethernet Switch (GMAC_SW).
    • DPLL_DSP: It feeds the DSP Subsystem clocking.
    • DPLL_GPU: It supplies clock for the GPU Subsystem.
    • DPLL_DDR: It generates clocks for the two External Memory Interface (EMIF) controllers and their
    associated EMIF PHYs.
    • DPLL_PCIE_REF: It provides reference clock for the APLL_PCIE in PCIE Subsystem.
    • APLL_PCIE: It feeds clocks for the device Peripheral Component Interconnect Express (PCIe)
    controllers.




    TDA 2H:

    DPLL_ABE
    DPLL_CORE
    DPLL_DEBUGSS
    DPLL_DSP
    DPLL_EVE
    DPLL_GMAC
    DPLL_HDMI
    DPLL_IVA
    DPLL_MPU
    DPLL_PER
    APLL_PCIE
    DPLL_PCIE_REF
    DPLL_SATA
    DPLL_USB
    DPLL_USB_OTG_SS
    DPLL_VIDEO1
    DPLL_VIDEO2
    DPLL_DDR
    DPLL_GPU

    Best Regards
  • Hi, ,

    Please, refer to PRCM chapter and corresponding chapters for DPLL functionality:

    Note that the PRCM chapter discusses only the DPLLs that are directly controlled by the PRCM module. The other DPLLs embedded in and managed by other subsystems are described in their respective subsystems.

    So, for example, DPLL_VIDEO1 is discussed in Display Subsystem Chapter.