Tool/software: Code Composer Studio
I am attempting to set up an ADS1298ECG FE Board with a TMS320C5515EVM. I am using CCS 4.1 and I am currently having a problem in getting the ECG SW loaded. Specifically, I get to the point where I am to load the ECG.out file and CCS4.1 reports that the .out file cannot be found and directing the software to look at a particular ECG.out file doesn't correct the issue. I am also having issues having the instructions from the CD that came with the C5515 EVM match with the actual CCS application. So, if anyone has a copy of the users guide/SW that actually match the C5515 EVM platform I am using, I would greatly appreciate it.