Part Number: AM3351
Tool/software: Linux
hi, i am using UART0 only, but evm have 6 uarts in dts file, i want to disable remaining uarts(1-5) after commenting in dts file i am getting below error, please suggest me what are the other places need to change.
aliases {
i2c0 = &i2c0;
i2c1 = &i2c1;
i2c2 = &i2c2;
serial0 = &uart0;
/*serial1 = &uart1; 06-11-17
serial2 = &uart2;
serial3 = &uart3;
serial4 = &uart4;
serial5 = &uart5;*/
d_can0 = &dcan0;
d_can1 = &dcan1;
usb0 = &usb0;
usb1 = &usb1;
phy0 = &usb0_phy;
phy1 = &usb1_phy;
ethernet0 = &cpsw_emac0;
ethernet1 = &cpsw_emac1;
};
///////error log//////
0.060009] CPU: Testing write buffer coherency: ok
[ 0.060809] Setting up static identity map for 0x80008200 - 0x80008258
[ 0.066004] devtmpfs: initialized
[ 0.092005] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
[ 0.109784] omap_hwmod: uart2: no dt node
[ 0.109830] ------------[ cut here ]------------
[ 0.109894] WARNING: CPU: 0 PID: 1 at arch/arm/mach-omap2/omap_hwmod.c:2533 _init.constprop.22+0x1fc/0x424()
[ 0.109913] omap_hwmod: uart2: doesn't have mpu register target base
[ 0.109928] Modules linked in:
[ 0.109970] CPU: 0 PID: 1 Comm: swapper Not tainted 4.4.12-g3639bea54a #9
[ 0.109991] Hardware name: Generic AM33XX (Flattened Device Tree)
[ 0.110006] Backtrace:
[ 0.110076] [<c00134e0>] (dump_backtrace) from [<c00136dc>] (show_stack+0x18/0x1c)
[ 0.110096] r7:c0770ad4 r6:000009e5 r5:00000009 r4:00000000
[ 0.110164] [<c00136c4>] (show_stack) from [<c02450a8>] (dump_stack+0x24/0x28)
[ 0.110212] [<c0245084>] (dump_stack) from [<c0031b4c>] (warn_slowpath_common+0x88/0xb4)
[ 0.110248] [<c0031ac4>] (warn_slowpath_common) from [<c0031bb0>] (warn_slowpath_fmt+0x38/0x40)
[ 0.110265] r8:00000081 r7:cf0b2380 r6:00000000 r5:00000000 r4:c06c6674
[ 0.110330] [<c0031b7c>] (warn_slowpath_fmt) from [<c0770ad4>] (_init.constprop.22+0x1fc/0x424)
[ 0.110347] r3:c06c7924 r2:c06c6674
[ 0.110371] r4:c07ac918
[ 0.110409] [<c07708d8>] (_init.constprop.22) from [<c0770e2c>] (__omap_hwmod_setup_all+0x48/0x98)
[ 0.110427] r10:00000000 r9:c0765600 r8:00000081 r7:cf0b2380 r6:c07a8ca0 r5:c07aab98
[ 0.110473] r4:c07ac918
[ 0.110510] [<c0770de4>] (__omap_hwmod_setup_all) from [<c00096bc>] (do_one_initcall+0x98/0x1e4)
[ 0.110527] r5:c0770de4 r4:c07a8ca0
[ 0.110591] [<c0009624>] (do_one_initcall) from [<c0765e80>] (kernel_init_freeable+0x138/0x1cc)
[ 0.110608] r10:00000002 r9:c0765600 r8:00000081 r7:c079681c r6:c07a2334 r5:c07db000
[ 0.110653] r4:c07db000
[ 0.110708] [<c0765d48>] (kernel_init_freeable) from [<c0582590>] (kernel_init+0x18/0xf4)
[ 0.110725] r10:00000000 r9:00000000 r8:00000000 r7:00000000 r6:00000000 r5:c0582578
[ 0.110769] r4:c07db000
[ 0.110806] [<c0582578>] (kernel_init) from [<c000fab8>] (ret_from_fork+0x14/0x3c)
[ 0.110823] r5:c0582578 r4:00000000
[ 0.110923] ---[ end trace e261df2aa2e3c1db ]---
[ 0.111520] omap_hwmod: uart3: no dt node
[ 0.111539] ------------[ cut here ]------------
[ 0.111582] WARNING: CPU: 0 PID: 1 at arch/arm/mach-omap2/omap_hwmod.c:2533 _init.constprop.22+0x1fc/0x424()
[ 0.111600] omap_hwmod: uart3: doesn't have mpu register target base
[ 0.111614] Modules linked in:
[ 0.111645] CPU: 0 PID: 1 Comm: swapper Tainted: G W 4.4.12-g3639bea54a #9
[ 0.111664] Hardware name: Generic AM33XX (Flattened Device Tree)
[ 0.111677] Backtrace:
[ 0.111721] [<c00134e0>] (dump_backtrace) from [<c00136dc>] (show_stack+0x18/0x1c)
[ 0.111739] r7:c0770ad4 r6:000009e5 r5:00000009 r4:00000000
[ 0.111797] [<c00136c4>] (show_stack) from [<c02450a8>] (dump_stack+0x24/0x28)
[ 0.111835] [<c0245084>] (dump_stack) from [<c0031b4c>] (warn_slowpath_common+0x88/0xb4)
[ 0.111870] [<c0031ac4>] (warn_slowpath_common) from [<c0031bb0>] (warn_slowpath_fmt+0x38/0x40)
[ 0.111887] r8:00000081 r7:cf0b2380 r6:00000000 r5:00000000 r4:c06c6674
[ 0.111950] [<c0031b7c>] (warn_slowpath_fmt) from [<c0770ad4>] (_init.constprop.22+0x1fc/0x424)
[ 0.111967] r3:c06c791c r2:c06c6674
[ 0.111990] r4:c07ac99c
[ 0.112028] [<c07708d8>] (_init.constprop.22) from [<c0770e2c>] (__omap_hwmod_setup_all+0x48/0x98)
[ 0.112046] r10:00000000 r9:c0765600 r8:00000081 r7:cf0b2380 r6:c07a8ca0 r5:c07aab98
[ 0.112090] r4:c07ac99c
[ 0.112126] [<c0770de4>] (__omap_hwmod_setup_all) from [<c00096bc>] (do_one_initcall+0x98/0x1e4)
[ 0.112143] r5:c0770de4 r4:c07a8ca0
[ 0.112190] [<c0009624>] (do_one_initcall) from [<c0765e80>] (kernel_init_freeable+0x138/0x1cc)
[ 0.112207] r10:00000002 r9:c0765600 r8:00000081 r7:c079681c r6:c07a2334 r5:c07db000
[ 0.112252] r4:c07db000
[ 0.112296] [<c0765d48>] (kernel_init_freeable) from [<c0582590>] (kernel_init+0x18/0xf4)
[ 0.112313] r10:00000000 r9:00000000 r8:00000000 r7:00000000 r6:00000000 r5:c0582578
[ 0.112357] r4:c07db000
[ 0.112394] [<c0582578>] (kernel_init) from [<c000fab8>] (ret_from_fork+0x14/0x3c)
[ 0.112411] r5:c0582578 r4:00000000
[ 0.112437] ---[ end trace e261df2aa2e3c1dc ]---
[ 0.112985] omap_hwmod: uart4: no dt node
[ 0.113001] ------------[ cut here ]------------
[ 0.113038] WARNING: CPU: 0 PID: 1 at arch/arm/mach-omap2/omap_hwmod.c:2533 _init.constprop.22+0x1fc/0x424()
[ 0.113057] omap_hwmod: uart4: doesn't have mpu register target base
[ 0.113070] Modules linked in:
[ 0.113099] CPU: 0 PID: 1 Comm: swapper Tainted: G W 4.4.12-g3639bea54a #9
[ 0.113117] Hardware name: Generic AM33XX (Flattened Device Tree)
[ 0.113130] Backtrace:
[ 0.113175] [<c00134e0>] (dump_backtrace) from [<c00136dc>] (show_stack+0x18/0x1c)
[ 0.113192] r7:c0770ad4 r6:000009e5 r5:00000009 r4:00000000
[ 0.113248] [<c00136c4>] (show_stack) from [<c02450a8>] (dump_stack+0x24/0x28)
[ 0.113285] [<c0245084>] (dump_stack) from [<c0031b4c>] (warn_slowpath_common+0x88/0xb4)
[ 0.113321] [<c0031ac4>] (warn_slowpath_common) from [<c0031bb0>] (warn_slowpath_fmt+0x38/0x40)
[ 0.113337] r8:00000081 r7:cf0b2380 r6:00000000 r5:00000000 r4:c06c6674
[ 0.113400] [<c0031b7c>] (warn_slowpath_fmt) from [<c0770ad4>] (_init.constprop.22+0x1fc/0x424)
[ 0.113418] r3:c06c7914 r2:c06c6674
[ 0.113441] r4:c07aca20
[ 0.113479] [<c07708d8>] (_init.constprop.22) from [<c0770e2c>] (__omap_hwmod_setup_all+0x48/0x98)
[ 0.113496] r10:00000000 r9:c0765600 r8:00000081 r7:cf0b2380 r6:c07a8ca0 r5:c07aab98
[ 0.113541] r4:c07aca20
[ 0.113577] [<c0770de4>] (__omap_hwmod_setup_all) from [<c00096bc>] (do_one_initcall+0x98/0x1e4)
[ 0.113594] r5:c0770de4 r4:c07a8ca0
[ 0.113639] [<c0009624>] (do_one_initcall) from [<c0765e80>] (kernel_init_freeable+0x138/0x1cc)
[ 0.113656] r10:00000002 r9:c0765600 r8:00000081 r7:c079681c r6:c07a2334 r5:c07db000
[ 0.113700] r4:c07db000
[ 0.113739] [<c0765d48>] (kernel_init_freeable) from [<c0582590>] (kernel_init+0x18/0xf4)
[ 0.113756] r10:00000000 r9:00000000 r8:00000000 r7:00000000 r6:00000000 r5:c0582578
[ 0.113800] r4:c07db000
[ 0.113836] [<c0582578>] (kernel_init) from [<c000fab8>] (ret_from_fork+0x14/0x3c)
[ 0.113853] r5:c0582578 r4:00000000
[ 0.113878] ---[ end trace e261df2aa2e3c1dd ]---
[ 0.114412] omap_hwmod: uart5: no dt node
[ 0.114428] ------------[ cut here ]------------
[ 0.114463] WARNING: CPU: 0 PID: 1 at arch/arm/mach-omap2/omap_hwmod.c:2533 _init.constprop.22+0x1fc/0x424()
[ 0.114481] omap_hwmod: uart5: doesn't have mpu register target base
[ 0.114493] Modules linked in:
[ 0.114522] CPU: 0 PID: 1 Comm: swapper Tainted: G W 4.4.12-g3639bea54a #9
[ 0.114539] Hardware name: Generic AM33XX (Flattened Device Tree)
[ 0.114552] Backtrace:
[ 0.114594] [<c00134e0>] (dump_backtrace) from [<c00136dc>] (show_stack+0x18/0x1c)
[ 0.114611] r7:c0770ad4 r6:000009e5 r5:00000009 r4:00000000
[ 0.114666] [<c00136c4>] (show_stack) from [<c02450a8>] (dump_stack+0x24/0x28)
[ 0.114702] [<c0245084>] (dump_stack) from [<c0031b4c>] (warn_slowpath_common+0x88/0xb4)
[ 0.114738] [<c0031ac4>] (warn_slowpath_common) from [<c0031bb0>] (warn_slowpath_fmt+0x38/0x40)
[ 0.114754] r8:00000081 r7:cf0b2380 r6:00000000 r5:00000000 r4:c06c6674
[ 0.114818] [<c0031b7c>] (warn_slowpath_fmt) from [<c0770ad4>] (_init.constprop.22+0x1fc/0x424)
[ 0.114835] r3:c06c790c r2:c06c6674
[ 0.114858] r4:c07acaa4
[ 0.114896] [<c07708d8>] (_init.constprop.22) from [<c0770e2c>] (__omap_hwmod_setup_all+0x48/0x98)
[ 0.114913] r10:00000000 r9:c0765600 r8:00000081 r7:cf0b2380 r6:c07a8ca0 r5:c07aab98
[ 0.114958] r4:c07acaa4
[ 0.114994] [<c0770de4>] (__omap_hwmod_setup_all) from [<c00096bc>] (do_one_initcall+0x98/0x1e4)
[ 0.115011] r5:c0770de4 r4:c07a8ca0
[ 0.115056] [<c0009624>] (do_one_initcall) from [<c0765e80>] (kernel_init_freeable+0x138/0x1cc)
[ 0.115073] r10:00000002 r9:c0765600 r8:00000081 r7:c079681c r6:c07a2334 r5:c07db000
[ 0.115118] r4:c07db000
[ 0.115157] [<c0765d48>] (kernel_init_freeable) from [<c0582590>] (kernel_init+0x18/0xf4)
[ 0.115174] r10:00000000 r9:00000000 r8:00000000 r7:00000000 r6:00000000 r5:c0582578
[ 0.115218] r4:c07db000
[ 0.115254] [<c0582578>] (kernel_init) from [<c000fab8>] (ret_from_fork+0x14/0x3c)
[ 0.115270] r5:c0582578 r4:00000000
[ 0.115295] ---[ end trace e261df2aa2e3c1de ]---
[ 0.115814] omap_hwmod: uart6: no dt node
[ 0.115829] ------------[ cut here ]------------
[ 0.115864] WARNING: CPU: 0 PID: 1 at arch/arm/mach-omap2/omap_hwmod.c:2533 _init.constprop.22+0x1fc/0x424()
[ 0.115882] omap_hwmod: uart6: doesn't have mpu register target base
[ 0.115895] Modules linked in:
[ 0.115923] CPU: 0 PID: 1 Comm: swapper Tainted: G W 4.4.12-g3639bea54a #9
[ 0.115941] Hardware name: Generic AM33XX (Flattened Device Tree)
[ 0.115954] Backtrace:
[ 0.115996] [<c00134e0>] (dump_backtrace) from [<c00136dc>] (show_stack+0x18/0x1c)
[ 0.116013] r7:c0770ad4 r6:000009e5 r5:00000009 r4:00000000
[ 0.116068] [<c00136c4>] (show_stack) from [<c02450a8>] (dump_stack+0x24/0x28)
[ 0.116104] [<c0245084>] (dump_stack) from [<c0031b4c>] (warn_slowpath_common+0x88/0xb4)
[ 0.116139] [<c0031ac4>] (warn_slowpath_common) from [<c0031bb0>] (warn_slowpath_fmt+0x38/0x40)
[ 0.116156] r8:00000081 r7:cf0b2380 r6:00000000 r5:00000000 r4:c06c6674
[ 0.116219] [<c0031b7c>] (warn_slowpath_fmt) from [<c0770ad4>] (_init.constprop.22+0x1fc/0x424)
[ 0.116236] r3:c06c78f0 r2:c06c6674
[ 0.116259] r4:c07acb28
[ 0.116297] [<c07708d8>] (_init.constprop.22) from [<c0770e2c>] (__omap_hwmod_setup_all+0x48/0x98)
[ 0.116313] r10:00000000 r9:c0765600 r8:00000081 r7:cf0b2380 r6:c07a8ca0 r5:c07aab98
[ 0.116359] r4:c07acb28
[ 0.116394] [<c0770de4>] (__omap_hwmod_setup_all) from [<c00096bc>] (do_one_initcall+0x98/0x1e4)
[ 0.116411] r5:c0770de4 r4:c07a8ca0
[ 0.116455] [<c0009624>] (do_one_initcall) from [<c0765e80>] (kernel_init_freeable+0x138/0x1cc)
[ 0.116472] r10:00000002 r9:c0765600 r8:00000081 r7:c079681c r6:c07a2334 r5:c07db000
[ 0.116517] r4:c07db000
[ 0.116557] [<c0765d48>] (kernel_init_freeable) from [<c0582590>] (kernel_init+0x18/0xf4)
[ 0.116574] r10:00000000 r9:00000000 r8:00000000 r7:00000000 r6:00000000 r5:c0582578
[ 0.116618] r4:c07db000
[ 0.116654] [<c0582578>] (kernel_init) from [<c000fab8>] (ret_from_fork+0x14/0x3c)
[ 0.116671] r5:c0582578 r4:00000000
[ 0.116695] ---[ end trace e261df2aa2e3c1df ]---
[ 0.129527] omap_hwmod: debugss: _wait_target_disable failed
[ 0.134474] omap_hwmod: d_can0: _wait_target_ready failed: -16
[ 0.134498] omap_hwmod: d_can0: cannot be enabled for reset (3)
[ 0.138424] omap_hwmod: d_can1: _wait_target_ready failed: -16
[ 0.138444] omap_hwmod: d_can1: cannot be enabled for reset (3)
[ 0.207577] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[ 0.212242] pinctrl core: initialized pinctrl subsystem
[ 0.215165] NET: Registered protocol family 16
[ 0.220504] DMA: preallocated 256 KiB pool for atomic coherent allocations
[ 0.247850] cpuidle: using governor ladder
[ 0.277829] cpuidle: using governor menu
[ 0.289180] OMAP GPIO hardware version 0.1
[ 0.292240] omap_gpio 481ac000.gpio: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/pinmux_gpio2_pins, deferrie
[ 0.292996] omap_gpio 481ae000.gpio: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/pinmux_gpio3_pins, deferrie
[ 0.311253] hw-breakpoint: debug architecture 0x4 unsupported.
[ 0.368323] edma 49000000.edma: TI EDMA DMA engine driver
[ 0.375875] usbcore: registered new interface driver usbfs
[ 0.376065] usbcore: registered new interface driver hub
[ 0.376328] usbcore: registered new device driver usb