Part Number: OMAP-L138
Hi, TI support!
I'm using TDU (Tone Detection Unit) from VOLIB Release 2.1.0.1. One of my task is to trace a call progress tones (CPT) at the voice channels.
The problem is, call progress tones could arrive from TDM side and from Network side simultaneously. But I need to trace only TDM tones. I have configured TDU to work only with TDM side and after conferencing (using tdu_CTL_POSITION). When CPT generated on the network side TDU is also activated, that is not required.
My question is how to configure tduCptCfgCtl_t (call progress tone detector configuration structure) to filter TDM side signal? There is no any such example in VOLIB packages. Parameters startFreq and endFreq are set to 420 Hz and 430 Hz accordingly. CPT on the both sides have the same frequency (425 Hz).
Many thanks!
Bakir