Other Parts Discussed in Thread: TDA2
Tool/software: Linux
Team,
Could you please answer the question from my customer.
Please find below his questions.
I’m not able to boot the DSPs of the TDA2+ outside SDK without using proprietary stuff.
The only two questions I have to ask:
What do I need to do so and where do I find the necessary code, like start-up snipped?
Are you able to give me a simple example?
The requirements I have to deal with:
1. Using cl6x toolchain is absolutely OK.
2. Build have to be embedded in a linux “Makefile” build environment, WITHOUT usage of XDC.
3. The Test-Chains of QM do not allow IDEs, such as CCS, so:
4. … Code must be compiled (assembled) ONLY in a Makefile environment
5. To handle Boot and Update processes: Linux runs on A15 core and will provide ALL SUBCORE STUFF using REMOTEPROC.
Goals:
Using only code which is REALLY necessary, so: Every line of code is desired and can be handled easy, managed in a simple boot-process.
SHORT: So absolutely bare-metal code have to meet linux remoteproc
I need:
Startup-code
Custom-Resource-table
With a proper Linker-cmd file
And of course: cl6x call -> How do I tell the compiler to create the “dra7-dsp1-fw.xe66” out of the just compiled obj linked together.
Thank you.
-Needhu