This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRA746: DDR termination on evm confirmation

Part Number: DRA746

Hello everybody , 

please some confirmation on DDR bus 

1-      Impedance of the DDR bus  : is it 40 or 50 ohm ?  you can see 47 on the evm

2-      DDR control/address bus  is   terminated   with 36  ohm on evm   :   is this correct ?

best regards

Carlo