This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Performance Issue H264Platinum Codec ( High Profile, Res-640x480 frame rate-10,15)

Hi,

i have integrated H264 Platinum Codec on DM365 based camera.

i am getting some problem with the video in 640x480 resolution.

i am getting flickering video on the lower half person.

i have attached the captured video.

can any one tell me what is the problem ?

is there any thing we need to do while setting up the codec static or dynamic parameters ?

or its a problem with Platinum Codec.

Specification for testing :

Resolution: 640*480

Framerate: 15 ( any resolution)

Compression: BEST

Bitrate Control: CBR

Target bitrate: 2048

Encoding Priority: Framerate

GOP size: 8 ( Any )

Profile: High

Entropy coding: CAVLC

 

h264PlatinumRecord.rar