Tool/software: Linux
Hello:
I compiled AM5728 platform's engineering using Qtcreator in the Ubuntu14.04 system, and the compiling error:
/home/linux/AM5728/linux-devkit/sysroots/armv7ahf-neon-linux-gnueabi/usr/include/gnu/stubs.h:7: error: gnu/stubs-soft.h: No such file or directory
# include <gnu/stubs-soft.h>
^
Looking forward to your professional reply, thank you!
The compile environment does not be checked out errors, and here is my installation environment:
1.Installed TI SDK ti-processor-sdk-linux-rt-am57xx-evm-03.03.00.04-Linux-x86-Install.bin to path:/home/linux/AM5728;
Installed cross compile file to path:/home/linux/gcc-linaro-5.3-2016.02-x86_64_arm-linux-gnueabihf;
Installed qt-creator-opensource-linux-x86_64-4.1.0.run to path: /home/linux/qtcreator-4.1.0.
2.Configuring Qt Creator
*Using TI SDK environment to enter Qt:
root@ubuntu:/home/linux# source /home/linux/AM5728/linux-devkit/environment-setup
[linux-devkit]:/home/linux> cd /home/linux/qtcreator-4.1.0/bin/
[linux-devkit]:/home/linux/qtcreator-4.1.0/bin> ./qtcreator
*Click Tool->Options->Build&Run->Compilers->Add->GCC:
compiler path: /home/linux/AM5728/linux-devkit/sysroots/x86_64-arago-linux/usr/bin/arm-linux-gnueabihf-g++;
*Click Tool->Options->Build&Run->Qt Versions->Add:
qmake location: /home/linux/AM5728/linux-devkit/sysroots/x86_64-arago-linux/usr/bin/qt5/qmake;
*Click Tool->Options->Build&Run->Debuggers->Add:
name: AM5728-Debugger
Path: /home/linux/gcc-linaro-5.3-2016.02-x86_64_arm-linux-gnueabihf/bin/arm-linux-gnueabihf-gdb
*Click Tool->Options->Build&Run->Kits->Add:
name:AM5728
Device type: Generic Linux Device
Compiler:GCC
Debugger:AM5728-Debugger
Qt version: Qt 5.6.2(qt5)
Once again, Looking forward to your professional reply, thank you!