This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SDK Setup.sh fails

My host OS version is ubuntu 14.04.1

After run the setup.sh, the failed informations as follows:

User 'root' is already apart of the 'dialout' group

-------------------------------------------------------------------------------
setup package script
This script will make sure you have the proper host support packages installed
This script requires administrator priviliges (sudo access) if packages are to be installed.
-------------------------------------------------------------------------------
System requires packages xinetd tftpd nfs-kernel-server build-essential libncurses5-dev automake dos2unix screen u-boot-tools to be installed
Installation requires you to have administrator priviliges (sudo access)
on your host. Do you have administrator privilieges?
Type 'y' to continue or 'n' to exit the installation: y
Performing sudo apt-get install xinetd tftpd nfs-kernel-server build-essential libncurses5-dev automake dos2unix screen u-boot-tools
Reading package lists... Done
Building dependency tree       
Reading state information... Done
You might want to run 'apt-get -f install' to correct these:
The following packages have unmet dependencies:
 automake : Depends: autoconf (>= 2.65) but it is not going to be installed
            Depends: autotools-dev (>= 20020320.1) but it is not going to be installed
 build-essential : Depends: gcc (>= 4:7.2) but 4:4.8.2-1ubuntu6 is to be installed
                   Depends: g++ (>= 4:7.2) but it is not going to be installed
                   Depends: dpkg-dev (>= 1.17.11) but it is not going to be installed
 libc-bin : Depends: libc6 (< 2.20) but 2.24-17 is to be installed
 libc-l10n : Breaks: locales (< 2.21-1) but 2.13+git20120306-12.1 is to be installed
 libc6 : Breaks: locales (< 2.24) but 2.13+git20120306-12.1 is to be installed
 libc6-dev : Depends: linux-libc-dev (>= 4.12.6) but 3.13.0-77.121 is to be installed
             Breaks: binutils (< 2.26) but 2.24-5ubuntu14 is to be installed
 libncurses5-dev : Depends: libtinfo5 (= 6.0+20170902-1) but 5.9+20140118-1ubuntu1 is to be installed
                   Depends: libncurses5 (= 6.0+20170902-1) but 5.9+20140118-1ubuntu1 is to be installed
                   Depends: libtinfo-dev (= 6.0+20170902-1) but it is not going to be installed
 nfs-kernel-server : Depends: libtirpc1 (>= 0.2.4) but it is not going to be installed
                     Depends: init-system-helpers (>= 1.18~) but 1.14 is to be installed
                     Depends: nfs-common (= 1:1.3.4-2.1+b1) but it is not going to be installed
                     Depends: keyutils
 screen : Depends: libtinfo5 (>= 6) but 5.9+20140118-1ubuntu1 is to be installed
E: Unmet dependencies. Try 'apt-get -f install' with no packages (or specify a solution).
Failed setup, aborting..
Failed setup, aborting..