Part Number: TMS320DM8127
Tool/software: Linux
Hi,
I use DM8127 CSK board. I use TI 8127 RDK 3.9.1 Release. From the documentation. This board has a DDR size of 2GB.
The u-boot detects this board as having only 1GB and not 2GB. When i run the memory tests the portion which access 0xA0000000 to 0xC0000000 hangs.
Can anyone provide clarity on this please? The only change i have done is to enable memory commands in the config file in u-boot.
Am i using the right sources or is this the expected behaviour?
My log:
U-Boot SPL 2016.05 (Nov 18 2017 - 20:15:17)
Trying to boot from MMC2
reading u-boot.img
reading u-boot.img
U-Boot 2016.05 (Nov 18 2017 - 20:15:17 +0530)
I2C: ready
DRAM: 1 GiB
MMC: OMAP SD/MMC: 0
Using default environment
Net: <ethaddr> not set. Reading from E-fuse
cpsw
Hit any key to stop autoboot: 0
DM8127-CSK# mtest 0x81000000 0xA0000000 0xaa55aa55 3
Testing 81000000 ... a0000000:
Pattern AA55AA55 Writing... Reading...Tested 3 iteration(s) with 0 errors.
DM8127-CSK# mtest 0xA0000000 0xC0000000 0xaa55aa55 3
Testing a0000000 ... c0000000:
Pattern AA55AA55 Writing...
Could you please advice me on this.
Thanks,
Sriram