This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/PROCESSOR-SDK-AM57X: Packages don't match in build

Part Number: PROCESSOR-SDK-AM57X
Other Parts Discussed in Thread: SYSBIOS

Tool/software: TI-RTOS

I opened a sysBios "hello world"  project in the C66 tab of the AM572x project wizard in the code composer. I attempted a build.

The builder, as you can see below is quite explicit. The default packages I installed  didn't match:

"C:/ti/xdctools_3_50_03_33_core/packages/xdc/cfg/Program.xs", line 71: xdc.cfg.Program : The package 'ti.sysbios.family.c64p' is not compatible with XDCtools used in this build. Please either use XDCtools compatible with that package, or update the product containing that package, or rebuild the package with XDCtools 3.50 or later.

I looked at the latest software in help[-> installation details and the numbers are correct. the xdc tools package and sysbios are as noted in the error message. Should I be pointing to a different xdc tools, and , is so, how do I switch pointers?