Other Parts Discussed in Thread: TVP5146, TVP5158
We have a 2 PAL/CBVS camera system.
The TPV5146 is set up for a single input and we have an external VIDEO MUX multiplexing the cameras. Both cameras are powered up. They are also out of sync with each other.
The DM355 and TVP5146 are wired up as per the EVM. Y2-Y9 to Y0-Y7 of the DM355. + PCLK
The CCDC is set up for BT.656 capture.
The aim of the product is to MUX the two cameras. and store a frame of each camera into memory ad infinitum.
We grab the 1st cameras frame and then switch to the second then back to the first etc.
When we look at the result, the frames are not vertically synchronised and sometimes not horizontally synched .
Q.
Is there a way to sync the VPFE when we switch to the next camera so that the ccdc is waiting for a New SAV ????
I am assuming that the TVP5146 will not have any time overheads appart from 1 or 2 frames.