Tool/software: TI-RTOS
Hi all
We are using emmc in Dra7xx-customized board.
we are getting the following info from /sys/kernel/debug. It shows 48 Mhz. the expected to be 192 Mhz . what is the maximum value support ?
cat mmc1/ios
clock: 48000000 Hz
vdd: 21 (3.3 ~ 3.4 V)
bus mode: 2 (push-pull)
chip select: 0 (don't care)
power mode: 2 (on)
bus width: 2 (4 bits)
timing spec: 9 (mmc HS200)
signal voltage: 0 (1.80 V)
driver type: 0 (driver type B)
Regards,
Gokul