This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CROPPING WHILE ROTATION

Hello,

I need a clarification about image rotation. If my image size is 1024 x 768 and my lcd resolution is 1280 x 768, what will happen if I rotate the image.

1. Will the image re-size it automatically and fit itself in the lcd screen?

2. If the engine does not re-size the image before rotation, will the image be cropped?

3. Else it is the duty of the developer to use re-sampling engine to down sample the image?

 

With regards,

Karthik.