Hi,
I am planning to boot 66AK2H14 SOC using NAND flash connected to EMIF interface, in one custom board.
For bootmode selection, I have provided switches for GPIO-01 to GPIO13 and CORESEL0, CORESEL1 & CORESEL2 pins so that these
pins can be set to either 1 or 0 at any time. But for GPIO-0 ( LENDIAN), GPIO14 ( MAINPLLODSEL), GPIO16 ( DDR3A_REMAP_EN)
and GPIO15 ( BOOTMODE_RSVD), I have not provided switch option and fixed these values to 0000. Please let me know whether
this setting is supported in evaluation module RTOS source code, for NAND flash booting.
Thanks & Regards,
Madhu