Hello. I use ti-processor-sdk-linux-am57xx-evm-03.03.00.04 and have some trouble with eth0.
I configured static IP 192.168.0.11 on eth0 and 192.168.0.12 on PC.
After connect cable I see message:
root@am57xx-evm:~# [ 997.825258] cpsw 48484000.ethernet eth0: Link is Up - 1Gbps/Full - flow control rx/tx
[ 997.833185] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
First, when I try ping sitara from PC:
ping 192.168.0.11
I gots "Destination Host Unreachable" messages.
Second, I ping PC from sitara:
ping 192.168.0.12
And got answers.
After, if I ping sitara from PC - got answers.
After reconnect cable - "Destination Host Unreachable" messages on PC, until sitara ping PC.
I.e. sitara not receive packets from eth0, until sitara try communicate with external host.
On eth1 this problem not exist.