Tool/software: Linux
Hi Sir
we follow below wiki to build the sdk and met the issue
OS: Ubuntu 14.04
we follow the command "MACHINE=am335x-evm bitbake arago-core-tisdk-image" and then it takes long time. finally it failed.
below is the log message. please advise and thanks
/home/ian/sdb1/tisdk/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/qtwebkit/5.7.1+gitAUTOINC+76e2732f01-r0.arago4/git/Source/WebCore/rendering/svg/RenderSVGAllInOne.cpp
compiling /home/ian/sdb1/tisdk/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/qtwebkit/5.7.1+gitAUTOINC+76e2732f01-r0.arago4/git/Source/WebCore/svg/SVGAllInOne.cpp
compiling /home/ian/sdb1/tisdk/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/qtwebkit/5.7.1+gitAUTOINC+76e2732f01-r0.arago4/git/Source/WebCore/accessibility/AccessibilityAllInOne.cpp
In file included from /home/ian/sdb1/tisdk/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/qtwebkit/5.7.1+gitAUTOINC+76e2732f01-r0.arago4/git/Source/WebCore/accessibility/AccessibilityAllInOne.cpp:44:0:
/home/ian/sdb1/tisdk/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/qtwebkit/5.7.1+gitAUTOINC+76e2732f01-r0.arago4/git/Source/WebCore/accessibility/AccessibilitySlider.cpp: In member function 'virtual void WebCore::AccessibilitySlider::addChildren()':
/home/ian/sdb1/tisdk/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/qtwebkit/5.7.1+gitAUTOINC+76e2732f01-r0.arago4/git/Source/WebCore/accessibility/AccessibilitySlider.cpp:81:6: warning: function might be candidate for attribute 'noreturn' [-Wsuggest-attribute=noreturn]
void AccessibilitySlider::addChildren()
^~~~~~~~~~~~~~~~~~~
compiling /home/ian/sdb1/tisdk/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/qtwebkit/5.7.1+gitAUTOINC+76e2732f01-r0.arago4/git/Source/WebCore/inspector/InspectorAllInOne.cpp
compiling /home/ian/sdb1/tisdk/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/qtwebkit/5.7.1+gitAUTOINC+76e2732f01-r0.arago4/git/Source/WebCore/loader/appcache/ApplicationCacheAllInOne.cpp
compiling /home/ian/sdb1/tisdk/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/qtwebkit/5.7.1+gitAUTOINC+76e2732f01-r0.arago4/git/Source/WebCore/platform/text/TextAllInOne.cpp
compiling /home/ian/sdb1/tisdk/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/qtwebkit/5.7.1+gitAUTOINC+76e2732f01-r0.arago4/git/Source/WebCore/rendering/style/StyleAllInOne.cpp
compiling /home/ian/sdb1/tisdk/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/qtwebkit/5.7.1+gitAUTOINC+76e2732f01-r0.arago4/git/Source/WebCore/html/HTMLElementsAllInOne.cpp
In file included from /home/ian/sdb1/tisdk/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/qtwebkit/5.7.1+gitAUTOINC+76e2732f01-r0.arago4/git/Source/WebCore/html/HTMLElementsAllInOne.cpp:54:0:
/home/ian/sdb1/tisdk/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/qtwebkit/5.7.1+gitAUTOINC+76e2732f01-r0.arago4/git/Source/WebCore/html/HTMLElement.cpp: In member function 'void WebCore::HTMLElement::setOuterText(const WTF::String&, WebCore::ExceptionCode&)':
/home/ian/sdb1/tisdk/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/qtwebkit/5.7.1+gitAUTOINC+76e2732f01-r0.arago4/git/Source/WebCore/html/HTMLElement.cpp:509:15: warning: nonnull argument 'this' compared to NULL [-Wnonnull-compare]
if (!this || !parentNode())
~~~~~~^~~~~~~~~~~~~~~~
compiling /home/ian/sdb1/tisdk/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/qtwebkit/5.7.1+gitAUTOINC+76e2732f01-r0.arago4/git/Source/WebCore/editing/EditingAllInOne.cpp
compiling /home/ian/sdb1/tisdk/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/qtwebkit/5.7.1+gitAUTOINC+76e2732f01-r0.arago4/git/Source/WebCore/rendering/RenderingAllInOne.cpp
In file included from /home/ian/sdb1/tisdk/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/qtwebkit/5.7.1+gitAUTOINC+76e2732f01-r0.arago4/git/Source/WebCore/rendering/RenderingAllInOne.cpp:47:0:
/home/ian/sdb1/tisdk/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/qtwebkit/5.7.1+gitAUTOINC+76e2732f01-r0.arago4/git/Source/WebCore/rendering/RenderBlock.cpp: In member function 'bool WebCore::RenderBlock::hasNextPage(WebCore::LayoutUnit, WebCore::RenderBlock::PageBoundaryRule) const':
/home/ian/sdb1/tisdk/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/qtwebkit/5.7.1+gitAUTOINC+76e2732f01-r0.arago4/git/Source/WebCore/rendering/RenderBlock.cpp:7403:59: warning: nonnull argument 'this' compared to NULL [-Wnonnull-compare]
RenderRegion* region = flowThread->regionAtBlockOffset(pageOffset, this);
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~^~~~~~~~~~~~~~~~~~
{standard input}: Assembler messages:
{standard input}:205351: Warning: end of file not at end of a line; newline inserted
{standard input}:205352: Error: missing expression -- `eor r4,'
compiling /home/ian/sdb1/tisdk/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/qtwebkit/5.7.1+gitAUTOINC+76e2732f01-r0.arago4/git/Source/WebCore/css/CSSAllInOne.cpp
arm-linux-gnueabihf-g++: internal compiler error: Killed (program cc1plus)
Please submit a full bug report,
with preprocessed source if appropriate.
See <gcc.gnu.org/bugs.html> for instructions.
make[2]: *** [.obj/inspector/InspectorAllInOne.o] Error 4
make[2]: *** Waiting for unfinished jobs....
make[2]: Leaving directory `/home/ian/sdb1/tisdk/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/qtwebkit/5.7.1+gitAUTOINC+76e2732f01-r0.arago4/build/Source/WebCore'
make[1]: *** [sub-Target-pri-make_first-ordered] Error 2
make[1]: Leaving directory `/home/ian/sdb1/tisdk/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/qtwebkit/5.7.1+gitAUTOINC+76e2732f01-r0.arago4/build/Source/WebCore'
make: *** [sub-Source-WebCore-WebCore-pro-make_first-ordered] Error 2
ERROR: Function failed: do_compile (log file is located at /home/ian/sdb1/tisdk/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/qtwebkit/5.7.1+gitAUTOINC+76e2732f01-r0.arago4/temp/log.do_compile.29668)
BR
Yimin