This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/AM5728: Custom board reboot issue

Part Number: AM5728


Tool/software: Linux

Hi all,

Recently,we designed a custom board for video capture use.Our board is booting from the eMMC,after the kernel start,it will reboot for several times,even worse,it may reboot endless.

We didn't use the RSTOUTn pin which GP EVM used for reset the board,our RSTOUTn pin is float,we also tried pull up the pin,it did't work.Is there any reboot mechanism in 5728 cause this issue.If so,what change should i make in sdk.I also found that the board reboot at nearly the same place shows below(the whole log file will be attached in the end).The kernel we used in eMMC is good in evm board and our old version board.The the PLSDK we used is ti-processor-sdk-linux-am57xx-evm-04.00.00.04.

Any insight on this will be welcome.

log file:reboot issue boot log.txt 


NOTE: If the package is a dependency of another package you
will be notified of the dependent packages. You should
use the --force-removal-of-dependent-packages option to
also remove the dependent packages as well
***************************************************************
***************************************************************
[ OK ] Started Print notice about GPLv3 packages.
[ 11.061955] FAT-fs (sda1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.
[ OK ] Started uim-sysfs.service.
Starting rc.pvr.service...
[ 11.194952] PVR_K: UM DDK-(3699939) and KM DDK-(3699939) match. [ OK ]
[ OK ] Started rc.pvr.service.
Starting weston.service...
[ OK ] Started weston.service.
Starting tiipclad-daemon.service...
Starting telnetd.service...
[ OK ] Started tiipclad-daemon.service.
[ OK ] Started telnetd.service.
Starting thttpd.service...
[ OK ] Started thttpd.service.
Starting rng-tools.service...
[ OK ] Started rng-tools.service.
Starting SYSV: The kdump script provides the support:...
[FAILED] Failed to start SYSV: The kdump script provides the support:.
See 'systemctl status kdump.service' for details.
Starting gdbserverproxy.service...
?
U-Boot SPL 2017.01-00319-gfe893f7-dirty (Nov 24 2017 - 23:57:07)
DRA752-GP ES2.0
Trying to boot from MMC2_2
Card did not respond to voltage select!
** Bad device mmc 0 **
Using default environment