Hi Guys,
we need to replace "DDR3 MT41K256M16HA-125:E" with "MT41K256M16TW-107:P" on AM3352 board.
According to AM335x TRM, the DDR3/3L maximum data rate is 800MHz..
Could we just apply the original configuration to new DDR3 chip?
If not, could you give some suggestions?
For example. CAS Latency of "MT41K256M16TW-107:P" is 13. And AM335x Max CAS Latency support is 11.
We have no idea how to configure for new DDR3 chip correctly.
Thanks.
Above diagram is from P.932@TI AM3352 TRM
Above diagram is from MICRON DDR3L SDRAM MT41K256M16TW-107:P SPEC
Regards,
ZL