Part Number: AM4376
Hi Sir
we used AM4376 for development and followed below wiki to do image building.
processors.wiki.ti.com/.../Processor_SDK_Building_The_SDK
we execute command "MACHINE=am437x-evm bitbake arago-base-tisdk-image" to build the image and found the speed is slow
linux-ti-staging-4.9.41+gitAUTOINC+e3a80a1c5c-r3c.arago5.tisdk9 do_fetch (pid 16328) 25% || 39.00 KiB/s
Q1: does Ti have any suggestion to improve the download speed (in china)
Q2 can we pre-download the source code and then integrate into tisdk folder ? if yes, can TI offer the document
BR
Yimin