This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM385: The CSI2 interface configuration

Part Number: DM385

Hello!

I want to connect the sony cmos sensor imx 230 to the dm385 processor by the mipi csi2 interface. I wonder that the configuration bellow is light?

CSI2_DX[0] ----------------------------------MIPI_CLK_n

CSI2_DY[0] ----------------------------------MIPI_CLK_p

CSI2_DX[1]---------------------------------- MIPI_DAT0_n

CSI2_DY[1]-----------------------------------MIPI_DAT0_p

.............

CSI2_DX[4]----------------------------------MIPI_DAT3_n

CSI2_DY[4]-----------------------------------MIPI_DAT3_p

The CSI2_DX[X] and the CSI2_DY[X] is from the DM385 datasheet in the device pin chapter. The MIPI_CLK is the clock lane of the CSI2 interface, and the MIPI_DATx is the data lane.